CAN43_FlexCAN generation error with CANFD and Enhanced FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN43_FlexCAN generation error with CANFD and Enhanced FIFO

1,322 Views
andamer
Contributor I

Hello, 

We're trying to use CANFD and Enhanched FIFO  on an s32k3 target with MCAL S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331 using S32DSstudio 

Version: 3.5
Build id: 230929 (Update 6)

And using Can43_flexcan in Autosar Mode.

But we are getting the following error in generation phase

andamer_0-1699519429270.pngandamer_0-1699519429270.png

Below some configurations 

andamer_1-1699519727153.pngandamer_1-1699519727153.png

 

andamer_2-1699519768731.pngandamer_2-1699519768731.png

 

 

 

0 Kudos
Reply
1 Reply

1,283 Views
NamLee
NXP Employee
NXP Employee

Hi andamer,

I think it's lack of resources. Please install the Service Pack 1 EAR4 as in Release Notes mentioned.

S32DS_pack1_EAR4.pngS32DS_pack1_EAR4.png

Please try to install another S32DS then the Service pack 1. I remember that user can't downgrade the DS-update version.

Thank you,

Nam.

0 Kudos
Reply