CAN TIME STAMP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN TIME STAMP

3,698 次查看
JackChen2022
Contributor I

Hello, I have a question to ask.The S32k148 chip is currently used, and the can communication is configured through the cal_pal component of the S32DS. Now I need to use the TIME STAMP function. I have learned about 53.4.3 Message buffer structure in the manual, but there is no specific usage method. I hope there is a usage routine or example.

0 项奖励
回复
5 回复数

3,686 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@JackChen2022

you can read the time stamp field from mailbox directly,

for example.

Senlent_1-1656489177910.png

 

0 项奖励
回复

3,676 次查看
JackChen2022
Contributor I

Thank you very much for your reply. I use SDK for development here, and register operation is not used. Do you have any other examples?

 

微信图片_20220630113433.png微信图片_20220630113627.png

0 项奖励
回复

3,656 次查看
KARTHKSARODE
Contributor III

Hi @JackChen2022 

To get the timestamp of the CAN message , you can read the CS of received CAN message and do AND operation with 0xFFFF , which will give the value of timestamp

timestamp=CS&0x0000FFFF; 

Best Regards
KARTHIK SV
0 项奖励
回复

3,636 次查看
JackChen2022
Contributor I

Thank you very much for your reply, the issue has been resolved

0 项奖励
回复

3,671 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@JackChen2022

I tried searching the internal system records and there is no such demo code for your reference.

As i said in my first reply, you can read the corresponding registers directly.

标记 (1)
0 项奖励
回复