CAN Receive with FreeRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Receive with FreeRTOS

2,305 Views
christofhaiding
Contributor IV

Hi everyone!

I am currently transporting the can_pal_S32K148 example to an FreeRTOS based project.

I created two different tasks, one for sending the other one for receiving

Sending in a separate Task is no problem.

But now i want to do some receiving.

Everything is fine as long as i use the Lines from the example project in my receive task:

/* Define receive buffer */
can_message_t recvMsg;

/* Start receiving data in RX_MAILBOX. */
CAN_Receive(&can_pal1_instance, RX_MAILBOX, &recvMsg);

/* Wait until the previous FlexCAN receive is completed */
while(CAN_GetTransferStatus(&can_pal1_instance, RX_MAILBOX) == STATUS_BUSY);

/* Check the received message ID and payload */
if((recvMsg.data[0] == LED0_CHANGE_REQUESTED) &&
recvMsg.id == RX_MSG_ID)
{
/* Toggle output value LED0 */
PINS_DRV_TogglePins(GPIO_PORT, (1 << LED0));
}
else if((recvMsg.data[0] == LED1_CHANGE_REQUESTED) &&
recvMsg.id == RX_MSG_ID)
{
/* Toggle output value LED1 */
PINS_DRV_TogglePins(GPIO_PORT, (1 << LED1));
}

If i send a data everything works without a problem.

But with this option I have the whole Idle time inside the while loop waiting for the state to get "unbusy", which I don't want to have.

So i tried to change it to something like this:

/* Start receiving data in RX_MAILBOX. */
CAN_Receive(&can_pal1_instance, RX_MAILBOX, &recvMsg);

/* Wait until the previous FlexCAN receive is completed */
if(CAN_GetTransferStatus(&can_pal1_instance, RX_MAILBOX) == STATUS_BUSY)

{

  return;

}

Because if i call this cyclic it should be the same like with the while, right?

Which works fine, if i send CAN Message with the wrong IDs.
But as soon as I send the CAN Message with the wright ID, for example 2 as done in the can_pal_S32K148 example, the whole system stops and I end up being stuck in the FreeRtos Watchdog.

I decreased the calling cycle to 1ms, which is the fastes cycle I can adjust at the FreeRTOS.

Is there any way to avoid this kind of error?

Or do I have to extract the CAN_GetTransferStatus function to some kind of IRQ and communicate with a flag that the can is not longer busy?

Best regards

Christof

 

 

 

 

Tags (2)
0 Kudos
Reply
3 Replies

2,273 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Christof,

I didn't see where you defined callback function for CAN_Receive by using CAN_InstallEventCallback. Would you please refer the S32K144_CAN_PAL_SamplePrj_Basic_TxRx_ID_FiltersConfig_SDKRTM3P0 example in S32K1xx SDK FlexCAN sample projects to demonstrate its basic and advanced features?
It will show you how to use callback instead of use CAN_GetTransferStatus.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,257 Views
christofhaiding
Contributor IV

Hi Robin!

I ported the sample code to my freeRTOS project and it works fine.

The key is to only call the CAN_Receive only once and wait until all data are there.

Thx for the support.

Regards 

Christof

0 Kudos
Reply

2,265 Views
christofhaiding
Contributor IV

Hi Robin, 

I didn't know that i have to use the function CAN_InstallEventCallback because it was not used at the sample project.

Thx for the tip, i will look into it.

Will come back to you when i have results.

Regards

Christof

0 Kudos
Reply