CAN FD configurations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FD configurations

1,250件の閲覧回数
Ayaz
Contributor IV

Hi

I am currently designing  the CAN FD configurations, and i have some doubts i like to share with you :

1)My PE clock is 40MHz. is it the CANCLK or Sclock ? 

Skærmbillede 2024-07-12 124506.pngSkærmbillede 2024-07-12 124523.png

2) Prescaler division factor , is it before added (+ 1) or after?

Skærmbillede 2024-07-12 124806.png Skærmbillede 2024-07-12 124919.png

3) if I want to configure bit timing for the nominal phase when the following are enabled for CAN FD. 

Skærmbillede 2024-07-12 145529.png

according to the RM i should follow the image below, right ?

Skærmbillede 2024-07-12 145836.png

4) when configuring  , which value do i  need to put , do i need to put the value for PSEG1 , FPSEG2 etc or the value of Time segments 1 and 2 ? Time quanta is it =  Time segment 1 + Time segment 2 ?

 Skærmbillede 2024-07-12 124806.png

0 件の賞賛
返信
1 返信

1,220件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Ayaz,

1) PE Clock refers to CANCLK.

2) Before Tq.

3) & 4) Please refer to

for bit timing calculation.

Best regards,
Julián

0 件の賞賛
返信