CAN-FD communication fail using TJA1145FD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN-FD communication fail using TJA1145FD

Jump to solution
3,006 Views
chengsz12060
Contributor II

Hello, NXP support,

Now I am debugging CAN-FD&TJA1145FD using s32k144. The phenomenon is as follows.
S32K144 + CAN-FD + TJA1043
→CAN-FD communication(send/receive) is successful.

S32K144 + CAN + TJA1145FD
→CAN communication(send/receive) is successful.

S32K144 + CAN-FD + TJA1145FD
→CAN communication fails.
→PC CAN Box Tool displays “error frame" in output window.
→TJA1145FD 's TX pin has waveform, but it is different from the waveform of CAN-FD&TJA1043.


<Question>
Why does the communication fail when MCU uses CAN-FD&TJA1145FD ?
Is there any difference in the control method or configuration method of TJA1145FD when MCU uses CAN and CAN-FD?

With Best Regards,

0 Kudos
Reply
1 Solution
2,986 Views
chengsz12060
Contributor II

I have checked the CFDC of  20h.

CAN-FD comunication fails if CFDC = 0.

CAN-FD communcaiton also fails if CFDC = 1.

20h.png

 

View solution in original post

0 Kudos
Reply
2 Replies
2,987 Views
chengsz12060
Contributor II

I have checked the CFDC of  20h.

CAN-FD comunication fails if CFDC = 0.

CAN-FD communcaiton also fails if CFDC = 1.

20h.png

 

0 Kudos
Reply
2,996 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi chengsz,

Please check the CFDC of CAN control and Transceiver status registers. Here is the Data Sheet of TJA1145.

TJA1145 CFDC.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply