CAN FD Bit Timing Calculation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FD Bit Timing Calculation

2,629件の閲覧回数
nitinverma
Contributor III

We are working on S32K144 board with REV1,
1. Clock source is BUS clock with 40Mhz frequency
2. Rx_Fifo = false
3. Fd_Enable = true
4. /* Macros to Configure Tx message buffer */
#define CANTX_DATALENGTH 64u
#define CANTX_FDENABLE 1u
#define CANTX_FDPADDING 0X00u
#define CANTX_ENABLEBRS 1u
The above mentioned values are passed in the function "FLEXCAN_DRV_ConfigTxMb"

/* Macros to Configure Rx message buffer */
#define CANRX_DATALENGTH 64u
#define CANRX_FDENABLE 1u
#define CANRX_FDPADDING 0u
#define CANRX_ENABLEBRS 1u
The above mentioned values are passed in the function "FLEXCAN_DRV_ConfigRxMb"

5. /* Macros for CAN_Baudrate setting for (CAN0->CBT with 500Kbps nominal bit rate) */
#define BAUDRATE_PROPSEG 46u
#define BAUDRATE_PHASESEG1 15u
#define BAUDRATE_PHASESEG2 15u
#define BAUDRATE_PREDIVIDER 0x00u
#define BAUDRATE_RJUMPWIDTH 15u

 

/* Macros for CAN_FD_Baudrate setting for (CAN0->FDCBT with 2Mbps higher bit rate)*/
#define BAUDRATE_PROPSEGFD 7u
#define BAUDRATE_PHASESEG1FD 7u
#define BAUDRATE_PHASESEG2FD 3u
#define BAUDRATE_PREDIVIDERFD 0x00u
#define BAUDRATE_RJUMPWIDTHFD 3u

With the above settings its working properly, Now I have S32K144 board with REV2,Clock source as FLEXCAN_CLK_SOURCE_SYS with 80Mhz frequency with SDK version as 0.9.0 . Please provide me the values needs to be passed for data bit rate of 2mbps and nominal bit rate of 500kbps. And also provide how the calculations will be done.

0 件の賞賛
返信
1 返信

2,055件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Nitin,

try to use following setting...

CBT = 0x802FBDEF;

FDCBT = 0x00131CE3;

FDCTRL[FDRATE]=1;

FDCTRL[TCDEN]=0;

BR, Petr

0 件の賞賛
返信