CAN BUS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN BUS

1,913件の閲覧回数
wutengyouxi555
Contributor II

wutengyouxi555_0-1708768900958.png

This function is canerr callback function from s32k144 SDK 4.0.2 

How CAN I know what kind of err has happened on the CAN bus from this Function.

0 件の賞賛
返信
3 返答(返信)

1,888件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

calling FLEXCAN_DRV_GetErrorStatus (reading ESR1) you clears status error bits. So read it into some status variable and mask/check as needed. You can refer to https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-TX-RX-Error-ISR-test-S32DS2...

BR, Petr 

1,876件の閲覧回数
wutengyouxi555
Contributor II
Thinks your help. One more question,if a CRC err occurs , could i know which message is this error coming from ?
0 件の賞賛
返信

1,864件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no, you have no such info about faulty message. Module does not store received CRC and moreover if error is detected a message is not moved-in into given MB. Just error free messages are stored, but without CRC info.

BR, Petr

0 件の賞賛
返信