Build error with S32K148EVB_LAN8651

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build error with S32K148EVB_LAN8651

511件の閲覧回数
yoneda
Contributor I

The following build error occurs with S32K148EVB_LAN8651. Could you please tell me the solution?
========

17:13:19 **** Build of configuration Debug_FLASH for project S32K148EVB_LAN8651 ****
make -j12 all
1 [main] make 1916 dofork: child -1 - forked process 7660 died unexpectedly, retry 0, exit code 0xC0000142, errno 11
make: *** [src/subdir.mk:57: src/DipSW.o] Error 127
"make -j12 all" terminated with exit code 2. Build might be incomplete.

17:13:20 Build Failed. 1 errors, 0 warnings. (took 711ms)

========

0 件の賞賛
返信
1 返信

472件の閲覧回数
RomanVR
NXP Employee
NXP Employee

Hi @yoneda.

To assist you further, could you please provide your project or describe its main functionality. From what I know the LAN8651 is an Ethernet interface that communicates via SPI protocol, but please confirm this is correct.

Aditionally, do you see the same behavior when loading any other projects onto the EVB?

I will be waiting for your response.

- RomanVR.

Best Regards!
0 件の賞賛
返信