Bricked PN5190 via NXP NFC Cockpit does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bricked PN5190 via NXP NFC Cockpit does not work

1,484 Views
zhouwenlu
Contributor I

Hello,

I have NXP S32K144EVB-Q100 board and NXP NCx3321 S32K Addon Board3, When updating Secure Upgrade to PN5190, The board doesnt work .

[2024.12.06 13:12:29]:INFO:BoardDetect:Enforcing board selection for PN5190
[2024.12.06 13:12:29]:INFO:ServiceFactory:Generating Services for VCOM_PN5190 @COM3
[2024.12.06 13:12:30]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:31]:WARN:OnlineVersionCheck:Please check your Internet connection!
[2024.12.06 13:12:31]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:32]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:33]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:34]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:34]:ERROR:ABalDelegate:Error while querying PIN_IRQ. GENERIC,USE_CONDITION
[2024.12.06 13:12:34]:WARN:ABalDelegate:Waited for PIN_IRQ to go High. Timed out.
[2024.12.06 13:12:35]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:36]:ERROR:ServiceFactory:InitHALPN5190.ApplyProtocolSettings failed. Status=240,IO_TIMEOUT
[2024.12.06 13:12:36]:ERROR:ServiceFactory:InitHALPN5190() failed. Status=240,IO_TIMEOUT
[2024.12.06 13:12:36]:ERROR:ServiceFactory:Previous FW Download to PN5190 seems to be incomplete. You may have to perform Secure FW Upgrade again
[2024.12.06 13:12:36]:INFO:SecureFWUpgrade:Entering download mode
[2024.12.06 13:12:37]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:38]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:39]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:40]:INFO:SecureFWUpgrade:Entered download mode
[2024.12.06 13:12:41]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:42]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:43]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:43]:ERROR:ABalDelegate:Error while querying PIN_BUSY. GENERIC,USE_CONDITION
[2024.12.06 13:12:43]:INFO:SecureFWUpgrade:Resetting Reader IC (FrontEnd) to enter normal mode
[2024.12.06 13:12:44]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:45]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:46]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:46]:INFO:SecureFWUpgrade:Reader IC (FrontEnd) Reset complete.
[2024.12.06 13:12:47]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:48]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:49]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:50]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:51]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:52]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:54]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:55]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:55]:INFO:ServiceFactory:Retrieved FW version from Secure Download Mode: 0.0
[2024.12.06 13:12:55]:ERROR:ServiceFactory:GenerateServices (VCOM_PN5190 @COM3) Failed with 240,IO_TIMEOUT
[2024.12.06 13:12:56]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:57]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:57]:INFO:ServiceFactory:uC FW Version: (Compiled on )
[2024.12.06 13:12:58]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:12:59]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:13:00]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:13:01]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:13:02]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:13:03]:ERROR:App:Internal Error occurred "The operation has timed out." in System
[2024.12.06 13:13:03]:ERROR:ServiceFactory:Bal, Hal, OSal Initialization (VCOM_PN5190 @COM3) Failed with 240,IO_TIMEOUT

zhouwenlu_0-1733462919995.png

 

0 Kudos
Reply
2 Replies

1,438 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @zhouwenlu 

Have you configured the COM port and baud rate correctly? It's recommended that you should follow the section 6.2 of UM789513 and try again.

0 Kudos
Reply

1,412 Views
zhouwenlu
Contributor I

This problem has been solved, is that the computer does not have USB read and write access to the problem, replace the computer has access to the problem has been solved!

Tags (1)
0 Kudos
Reply