Bootloader S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader S32K3

1,377 Views
enthuCutlet
Contributor II

Bootloader not going into application code and is presenting with a hard fault. Even after using the correct address of the reset handler the problem still persists

0 Kudos
Reply
1 Reply

1,345 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @enthuCutlet 

if you step the jump command using asm instruction stepping (do not use stepping in C, it's useless here), can you see if it jumps to entry point of the application? It usually does jump to the entry point. And it usually fails later in the code due to insufficient de-initialization.

So, first step is to check if it jumps to the entry point or not.

Regards,

Lukas

0 Kudos
Reply