Bootloader|| Device Jump to application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader|| Device Jump to application

3,778件の閲覧回数
shubhendu_shukl
Contributor II

Hi,

IDE: IAR

Controller s32k144

bootloader interface: UART

As mentioned in AN12218 I have made changes in bootloader it is also working one time(I am able to update application code one time)

But whenever I am trying to update different image(making some changes in same application code),the code is getting stuck in unknown memory location.

Can Anyone tell me why is it happening and What changes do I need to make to avoid this issue.

*I am using the same bootloader code provided by NXP for bootloader by UART.

ラベル(1)
5 返答(返信)

3,534件の閲覧回数
shubhendu_shukl
Contributor II

Hi Diana,

We have identified the issue, we were not erasing the sectors properly after changing the application begin address. Bootloader is up and running now.

3,534件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Which changes have you made?

Can you share your .srec file?

Thank you.

Best regards,

Diana

0 件の賞賛
返信

3,534件の閲覧回数
w_lingjun
Contributor III

Hi Diana,

I'm working on FBL development too, I asked  you some flash problems several days ago. I've program the app code into flash by FBL successfully, but after boot, I can't start app because it will get stuck in WDOG_EWM_IRQHandler();

Is this the app code or the FBL code problem?

error.png

Best regards,

Sarah

0 件の賞賛
返信

3,534件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Sarah,

I'm sorry for the delay.

I recommend you to look at the link https://community.nxp.com/docs/DOC-334902 

You can create a HardFault handler and debug the exception.

Best regards,

Diana

0 件の賞賛
返信

3,534件の閲覧回数
w_lingjun
Contributor III

Hi Diana,

I click the link you supplied, then enter the following link is error.

link.png

err1.png

Is there anywhere I can get the fault handling example?

Best regards,

Sarah

0 件の賞賛
返信