BSDL File for S32K142 in LQFP64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSDL File for S32K142 in LQFP64

Jump to solution
3,592 Views
guenter_loettrich
NXP Employee
NXP Employee

Hi,

can someone send me the BSDL file for S32K142 in LQFP64, please?

When using the file for S32K144 (s32k144_lqfp64_993C01D.bsdl) it doesn't work because the BoundaryScan Register description is too long.

br

Guenter

0 Kudos
Reply
1 Solution
3,403 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Guenter,

I will send you the file.

Regards,

Daniel

View solution in original post

4 Replies
3,404 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Guenter,

I will send you the file.

Regards,

Daniel

1,606 Views
Octavio
Contributor I
Hello, I need the same BSDL file, could you plase send to me too.

Regards,
Octavio
0 Kudos
Reply
2,896 Views
Allela_ICT
Contributor I

Hello  , 

Precisely I need the BSDL file for  the micro is : FS32K142HFT0VLLR 105C LQFP100 .

Thanks 

0 Kudos
Reply
2,899 Views
Allela_ICT
Contributor I

Hello  , 

I need the BSDL file for S32K142HFT0 , would you please send me the link to download ? 

 

Regards 

Allela 

0 Kudos
Reply