BSDL File for S32K142 in LQFP64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSDL File for S32K142 in LQFP64

ソリューションへジャンプ
3,593件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi,

can someone send me the BSDL file for S32K142 in LQFP64, please?

When using the file for S32K144 (s32k144_lqfp64_993C01D.bsdl) it doesn't work because the BoundaryScan Register description is too long.

br

Guenter

0 件の賞賛
返信
1 解決策
3,404件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Guenter,

I will send you the file.

Regards,

Daniel

元の投稿で解決策を見る

4 返答(返信)
3,405件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Guenter,

I will send you the file.

Regards,

Daniel

1,607件の閲覧回数
Octavio
Contributor I
Hello, I need the same BSDL file, could you plase send to me too.

Regards,
Octavio
0 件の賞賛
返信
2,897件の閲覧回数
Allela_ICT
Contributor I

Hello  , 

Precisely I need the BSDL file for  the micro is : FS32K142HFT0VLLR 105C LQFP100 .

Thanks 

0 件の賞賛
返信
2,900件の閲覧回数
Allela_ICT
Contributor I

Hello  , 

I need the BSDL file for S32K142HFT0 , would you please send me the link to download ? 

 

Regards 

Allela 

0 件の賞賛
返信