BCTU List Configuration in ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BCTU List Configuration in ADC

3,504件の閲覧回数
Mithulesh23
Contributor II

Hi Team,

@PetrS 

I am configured some pins for BCTU Hardware trigger as List items. And I need to configure some additional pins. But,It shows watermark limit reached. I cannot set the value more than 7.

Mithulesh23_1-1712573725180.png

 

Mithulesh23_2-1712573877767.png

Please assist on this issue.

Thank you

0 件の賞賛
返信
6 返答(返信)

3,432件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Mithulesh23

The size of FIFO2 only have 8 words and you can't set the FIFO2 watermark value more than 7.

 

S32K3XXRM_rev8->Chapter 65.

Senlent_0-1712813678845.png

 

0 件の賞賛
返信

3,426件の閲覧回数
Mithulesh23
Contributor II

@Senlent ,

Thank you for the clarification.

So, we can be able to create totally 24 channels in the list for ADC BCTU. Please confirm.

 

タグ(1)
0 件の賞賛
返信

3,419件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Mithulesh23

yes, you can create 24 channels in the list.

What does "Watermark" do : 

Senlent_0-1712817008039.png

 

 

0 件の賞賛
返信

3,398件の閲覧回数
Mithulesh23
Contributor II

@Senlent,

Thank you for confirming it.

I have already configured 16 channels in the BCTU list.

 

Mithulesh23_0-1712830640994.png

Mithulesh23_1-1712830841435.png

 

Mithulesh23_2-1712830876091.png

 

Now, in the next list I'm trying to configure below listed 8 channels. As the FIFO2 size limit is 8, please help me to configure with below combinations.

ADC0_S15
ADC0_S14
ADC0_S13
ADC0_S12
ADC0_S11
ADC0_S18

 

ADC1_S16
ADC1_S18

Thank you

タグ(1)
0 件の賞賛
返信

3,361件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Mithulesh23

Please refer to the sample project in the link below which is the same as your requirement.

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-...

 

0 件の賞賛
返信

3,479件の閲覧回数
Dev15
Contributor III

@Senlent , 

Please assist on this configuration.

Thank you

タグ(1)
0 件の賞賛
返信