Hi @namnguyenviet_001
In standard single-bit SPI operation, the bit rate (in Mbps) is numerically equal to the SPI clock frequency (in MHz), since one bit is transferred per clock cycle.
Regarding Master Loopback mode (available only for LPSPI0), as described in notes 5 and 6 below Table 46 of the S32K1xx Data Sheet, Rev. 15, the LPSPI_SCK clock can be delayed for input data sampling by enabling the LPSPI_CFGR1[SAMPLE] bit. This feature improves the setup time of the received data path, allowing operation at higher baud rates.
The following simplified diagram of how the CFGR1[SAMPLE] feature works:

BR, VaneB