Adding LinkServer debugging to S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding LinkServer debugging to S32DS

2,709件の閲覧回数
maksym_leski
Contributor I

Hello, I have a question due to debugging problems with my probe. I have CMSIS-DAP probe based on LPC11U35 uC. The MCUXpresso software detect's it as LinkServer probe, and works fine. I would like to add that debugging configuration to S32DS platform to debug S32K144 with it. Is that possible? I read threads like this https://community.nxp.com/t5/S32-Design-Studio/Debugger-options-for-S32DS/td-p/648501 but it's not working.

Would apprecitate any help

0 件の賞賛
返信
2 返答(返信)

2,694件の閲覧回数
maksym_leski
Contributor I

thank you Robin_Shen for your reply.

I tried very different ways to make it work, even I tried to make fresh Eclipse workbench including S32DS features along with MCUXpresso features, but none of them succeed. Guess that I need to buy some other probe. 

best regards,

Max

0 件の賞賛
返信

2,701件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi maksym_leski,

Sorry, this debug probe is not in the support list of S32 Design Studio for S32 Platform 3.4, so you can not achieve it.
You can find the Supported hardware debug probes in S32DS_User_Guide.

Supported hardware debug probes.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信