AUTOSAR control LED toggle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR control LED toggle

2,468 Views
gravity_one
Contributor III

hi,

use S32K148  +  AUTOSAR  control  PTE-21.22.23  LED toggle.

i do not konw  how to do ?

step1: EB_tresos tool  generate  AUTOSAR_code.

step2: porting AUTOSAR_code to S32DS .

step3: integrated development on  S32DS.

But I try to generate AUTOSAR_code are NULL , feel like useless functions.


#ifdef __cplusplus
extern "C" {
#endif

/*=================================================================================================
* INCLUDE FILES
* 1) system and project includes
* 2) needed interfaces from external units
* 3) internal and external interfaces from this unit
=================================================================================================*/

#include "Dio.h"


#if (defined(DIO_PRECOMPILE_SUPPORT) || defined(DIO_LINKTIME_SUPPORT))
/*=================================================================================================
* SOURCE FILE VERSION INFORMATION
=================================================================================================*/

#define DIO_VENDOR_ID_CFG_C 43
/** @violates @ref Dio_Cfg_C_REF_1 The used compilers use more than 31 chars for identifiers. */
#define DIO_AR_RELEASE_MAJOR_VERSION_CFG_C 4
/** @violates @ref Dio_Cfg_C_REF_1 The used compilers use more than 31 chars for identifiers. */
#define DIO_AR_RELEASE_MINOR_VERSION_CFG_C 3
/** @violates @ref Dio_Cfg_C_REF_1 The used compilers use more than 31 chars for identifiers. */
#define DIO_AR_RELEASE_REVISION_VERSION_CFG_C 1
#define DIO_SW_MAJOR_VERSION_CFG_C 1
#define DIO_SW_MINOR_VERSION_CFG_C 0
#define DIO_SW_PATCH_VERSION_CFG_C 1

/*=================================================================================================
* FILE VERSION CHECKS
=================================================================================================*/


#if (((DIO_AR_RELEASE_MAJOR_VERSION_CFG_C != DIO_AR_RELEASE_MAJOR_VERSION) || \
(DIO_AR_RELEASE_MINOR_VERSION_CFG_C != DIO_AR_RELEASE_MINOR_VERSION) \
) || \
(DIO_AR_RELEASE_REVISION_VERSION_CFG_C != DIO_AR_RELEASE_REVISION_VERSION)\
)
#error "AutoSar Version Numbers of Dio_Cfg.c and Dio.h are different"
#endif
#if ((DIO_SW_MAJOR_VERSION_CFG_C != DIO_SW_MAJOR_VERSION) || \
(DIO_SW_MINOR_VERSION_CFG_C != DIO_SW_MINOR_VERSION) || \
(DIO_SW_PATCH_VERSION_CFG_C != DIO_SW_PATCH_VERSION) \
)
#error "Software Version Numbers of Dio_Cfg.c and Dio.h are different"
#endif
#if ((DIO_VENDOR_ID_CFG_C != DIO_VENDOR_ID))
#error "VENDOR ID for Dio_Cfg.c and Dio.h is different"
#endif

/*=================================================================================================
* LOCAL TYPEDEFS (STRUCTURES, UNIONS, ENUMS)
=================================================================================================*/


/*=================================================================================================
* LOCAL MACROS
=================================================================================================*/


/*=================================================================================================
* LOCAL CONSTANTS
=================================================================================================*/


/*=================================================================================================
* LOCAL VARIABLES
=================================================================================================*/


/*=================================================================================================
* GLOBAL CONSTANTS
=================================================================================================*/

#define DIO_START_SEC_CONFIG_DATA_UNSPECIFIED

/** @violates @ref Dio_Cfg_C_REF_2 MISRA 2004 Required Rule 19.15,
Precautions to prevent the contents of a header file being included twice.*/
#include "Dio_MemMap.h"

/**
* @brief Platform implemented port pins representation.
* @details Array of bit maps reflecting the available pins in each port.
* The number of elements in the array corresponds to the number of
* ports implemented in the platform package. Rightmost bit of each
* array element corresponds to channel 0 of the associated port,
* while leftmost bit of each array element corresponds to channel 31
* of the associated port. A 0 bit means that the correspondent channel
* is not available in the platform package, while a bit of 1 means
* that the correspondent channel is available in the platform package.
*
* @api
*/
/** @violates @ref Dio_Cfg_C_REF_4 This warning appears when defining functions or objects that will be used by the upper layers. */
CONST(Dio_PortLevelType, DIO_CONST) Dio_aAvailablePinsForWrite[DIO_NUM_PORTS_U16] =
{
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0x0FFFFFFFUL
};

/** @violates @ref Dio_Cfg_C_REF_4 This warning appears when defining functions or objects that will be used by the upper layers. */
CONST(Dio_PortLevelType, DIO_CONST) Dio_aAvailablePinsForRead[DIO_NUM_PORTS_U16] =
{
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0xFFFFFFFFUL,
(Dio_PortLevelType)0x0FFFFFFFUL
};


/* ========== DioConfig ========== */


/**
* @brief Data structure for configuration DioConfig.
*/
/** @violates @ref Dio_Cfg_C_REF_4 This warning appears when defining functions or objects that will be used by the upper layers. */
CONST(Dio_ConfigType, DIO_CONST) DioConfig =
{
(uint8)0x0,
NULL_PTR

};


#define DIO_STOP_SEC_CONFIG_DATA_UNSPECIFIED

/** @violates @ref Dio_Cfg_C_REF_2 MISRA 2004 Required Rule 19.15,
Precautions to prevent the contents of a header file being included twice.*/
/** @violates @ref Dio_Cfg_C_REF_3 MISRA 2004 Advisory Rule 19.1,
Only preprocessor statements and comments before '#include'.*/
#include "Dio_MemMap.h"

/*=================================================================================================
* GLOBAL VARIABLES
=================================================================================================*/


/*=================================================================================================
* LOCAL FUNCTION PROTOTYPES
=================================================================================================*/


/*=================================================================================================
* LOCAL FUNCTIONS
=================================================================================================*/


/*=================================================================================================
* GLOBAL FUNCTIONS
=================================================================================================*/


#endif /* (defined(DIO_PRECOMPILE_SUPPORT) || defined(DIO_LINKTIME_SUPPORT)) */

#ifdef __cplusplus
}
#endif

/** @} */

13.png

BRS 

Grayli

0 Kudos
Reply
1 Reply

2,348 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello WANG LI,

I see that you just configure one "DIO channel" and do not have any "DIO channel group".

So the generated code in file Dio_Cfg.c will be:

CONST(Dio_ConfigType, DIO_CONST) DioConfig =
{
(uint8)0x0,
NULL_PTR

};

because this variable is used for "DIO channel group" (function Dio_ReadChannelGroup and Dio_WriteChannelGroup)

The configuration you set for "DIO channel" just effect to file Dio_Cfg.h:

#define  DioConf_DioChannel_DioChannel_0 ((uint16)0x0015U)

and it will use as input of function  Dio_ReadChannel or Dio_WriteChannel.

0 Kudos
Reply