AUTOSAR Can module can not receive standard signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AUTOSAR Can module can not receive standard signal

ソリューションへジャンプ
2,159件の閲覧回数
郑文豪
Contributor I

AUTOSAR Can module can not receive standard signal when Can ID message Type is set to Mixed in S32K1XX MCAL,but Extended ID can.Why cannot receive standard signal when Can ID message Type is set to Mixed?LRVHI6MI]$G0ABUIBGP9246.png

0 件の賞賛
返信
1 解決策
2,131件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Unfortunately, "Mixed" and "Extended" are implemented with the same behavior, as it's a deviation noted in CAN UM:

 "The driver does not distinguish between “Extended” and “Mixed” MB types for receiving way: All Rx MBs configured as MIXED type will be converted to EXTENDED type. For transmission the CanIf will prepare the message ID with MSB bit set and based on this fact the Can module will send the message as STANDARD or EXTENDED type. See CANIF188 and CANIF281 requirements"

Best Regards,

Nam

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,132件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

Unfortunately, "Mixed" and "Extended" are implemented with the same behavior, as it's a deviation noted in CAN UM:

 "The driver does not distinguish between “Extended” and “Mixed” MB types for receiving way: All Rx MBs configured as MIXED type will be converted to EXTENDED type. For transmission the CanIf will prepare the message ID with MSB bit set and based on this fact the Can module will send the message as STANDARD or EXTENDED type. See CANIF188 and CANIF281 requirements"

Best Regards,

Nam

0 件の賞賛
返信