Hello,
I am using S32k144 and i want to configure ADC to be triggered with PDB timer which got triggered with TriggerMux.
I want to use ADC without polling for the COCO flag, and without interrupts also, just a timer triggers pdb timer which triggers.
I have some questions:
1- To be able to do that, is it mandatory to configure ADC to work with DMA?
2- If not, am i getting the idea right? if yes, how should the configuration process go?
3- Is there an example for that?
That's for now, appreciate your kind support.
Thank you.