ADC external channel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,975件の閲覧回数
David_Qin___1
Contributor I

Hello, 

How do I know which ADC_INPUTCHAN_EXTx is connected to ADCx_SExx when I use the Processor Expert?   i can't find the details in the reference manual. Thanks!

Oliver_Zhang_1-1640137345652.pngOliver_Zhang_2-1640137387560.png

 

タグ(1)
0 件の賞賛
返信
1 解決策
2,968件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oliver_zhang

ADC_INPUTCHAN_EXT3 -> ADC0-SE3

ADC_INPUTCHAN_EXT4 -> ADC0-SE4

...........and so on.

 

for example:S32K142-> Configurate PTC14 to ADC port.

PTC14 related to ADC0-channel12-> ADC_INPUTCHAN_EXT12.

BR!

     Jim,

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,969件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Oliver_zhang

ADC_INPUTCHAN_EXT3 -> ADC0-SE3

ADC_INPUTCHAN_EXT4 -> ADC0-SE4

...........and so on.

 

for example:S32K142-> Configurate PTC14 to ADC port.

PTC14 related to ADC0-channel12-> ADC_INPUTCHAN_EXT12.

BR!

     Jim,

 

0 件の賞賛
返信
2,962件の閲覧回数
David_Qin___1
Contributor I

Thank you sir! 

0 件の賞賛
返信