ADC conversion of more than 8 external channels using S32K118 using PDB and DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ADC conversion of more than 8 external channels using S32K118 using PDB and DMA

跳至解决方案
636 次查看
francescovico
Contributor III

Hello, I need to make ADC conversion of 10 external channels reducing load of CPU.

My problem it's that S32K118 have 1 ADC and 1 PDB that could only trigger 8 different channels of ADC.

There is a configuration that could convert 10 channels  reducing load of CPU  ?

Regards, Francesco.

0 项奖励
回复
1 解答
606 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

There is no an example for the S32K118, but you could refer to the following post:

Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1

Where 2 ADC modules and 2 PDBs are used, but specifically the ADC0 is configured to sample 16 channels.

Hope it helps you.

Have a nice day!

在原帖中查看解决方案

0 项奖励
回复
1 回复
607 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

There is no an example for the S32K118, but you could refer to the following post:

Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1

Where 2 ADC modules and 2 PDBs are used, but specifically the ADC0 is configured to sample 16 channels.

Hope it helps you.

Have a nice day!

0 项奖励
回复