ADC conversion, MCU hardFaulted when used with CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC conversion, MCU hardFaulted when used with CAN

1,077 Views
Lily_31_amz
Contributor II

Hello NXP Team,

i can convert ADC values without issue using the example coming with the SDK.

i have a requirement that when the controller receive a CAN message it should do an ADC conversion and return back the result in other CAN message.

the MCU do this in first attempt,and i get a CAN respond back with the correct ADC values, but when i send the command the second time the MCU stops at a hard fault (ADC0_IRQHandler).

here is my code for ADC

 

void adc1_init(void)
{
	/* Enable the floating point unit et both CPACR[CP11] and CPACR[CP10] to Full Access - 0b11 */
    S32_SCB->CPACR |= (S32_SCB_CPACR_CP10_MASK | S32_SCB_CPACR_CP11_MASK);

    /* Get ADC max value from the resolution */
    if (adConv1_ConvConfig0.resolution == ADC_RESOLUTION_8BIT)
        adcMax = (uint16_t) (1 << 8);
    else if (adConv1_ConvConfig0.resolution == ADC_RESOLUTION_10BIT)
        adcMax = (uint16_t) (1 << 10);
    else
        adcMax = (uint16_t) (1 << 12);

    ADC_DRV_ConfigConverter(INST_ADCONV1, &adConv1_ConvConfig0);
    ADC_DRV_AutoCalibration(INST_ADCONV1);
    INT_SYS_SetPriority(ADC0_IRQn,configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY);

}

void TEST_KL15_AD(uint16_t *adcVal)
{
	float adcValue = 0.0f;
	uint16_t adcRawValue = 0U;

	/* Configure ADC channel and software trigger a conversion */
	ADC_DRV_ConfigChan(INST_ADCONV1, 0U, &adConv_KL15_ch10);
    /* Wait for the conversion to be done */
    ADC_DRV_WaitConvDone(INST_ADCONV1);
    /* Store the channel result into a local variable */
    ADC_DRV_GetChanResult(INST_ADCONV1, 0U, &adcRawValue);

    /* Process the result to get the value in volts */
    adcValue = ((float) adcRawValue / adcMax) * (ADC_VREFH - ADC_VREFL);

    printf("KL15_AD: %f\r\n", adcValue);

    *adcVal = FLOAT_TO_INT(adcValue);

}

 

 

i task call the adc1_init() , and in the loop we read if we have a valid CAN message in the mailbox.

 

 

void canCyclic(void *pvParameters)
{
	 (void)pvParameters;

	 // initialize the SBC and CAN driver
	can_driver_init();

	// initialize ADC 
	adc1_init();

	while(1)
	{
		can_read_MailBox();
		
		vTaskDelay(10/portTICK_PERIOD_MS);
	}
}

void can_read_MailBox(){

	flexcan_msgbuff_t recvBuff;
	status_t rx_ret_value = STATUS_UNSUPPORTED;
	uint8_t RX_MAILBOX = 0;

	/* Start receiving data in RX_MAILBOX. */
	rx_ret_value = FLEXCAN_DRV_Receive(INST_CANCOM1, RX_MAILBOX, &recvBuff);

	if(rx_ret_value == STATUS_SUCCESS)
	{
		can_rx_interpreter(recvBuff);
	}
}
void can_rx_interpreter(flexcan_msgbuff_t rxCanMessage)
{

switch(rxCanMessage.msgId)
	{
		case Read_TCU_Analog_IN:

                uint8_t dataOut[8];
		
                memset(dataOut, 0, 8);
			uint16_t kl15_ad_value = 0U;

			TEST_KL15_AD(&kl15_ad_value);

			dataOut[0] = (kl15_ad_value >>  & 0xFF;
			dataOut[1] = (kl15_ad_value) & 0xFF;

			can_Transmit_Results(2,TCU_Analog_IN_D,dataOut,8);

			break;
		default:
			printf("id not supported \r\n");
			break;
}
}

 

 

 

Thank you.

0 Kudos
Reply
1 Reply

1,071 Views
Lily_31_amz
Contributor II

it turn out that the problem reside in this line 

*adcVal = (uint16_t)(adcValue);

the compiler does not give error, but when executed the runtime stops !

is there a convenient way to convert from Float to uint ?

Thank you.

0 Kudos
Reply