ADC calibration by using Calibration Averaging method

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC calibration by using Calibration Averaging method

989 Views
Venu_M
Contributor III

 Hello NXP team,

              I  want to do calibrate the ADC results by using  Adc_Calibrate(), I can able to do the 32samples only, not able to change the any other samples .

Venukumar_0-1693585014925.png

 

Venukumar_1-1693585064965.png


If i want to change the sample count from 32 to 16 or 8 , whether i need to change the bit position manually in the Adc_Sar_Ip.c?

 

Tags (1)
0 Kudos
Reply
1 Reply

948 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

As far as I know ADC performance specifications are guaranteed when calibration uses maximum averaging i.e. when AVGEN = 1 and AVGS = 3. This is why Adc_Calibrate uses 32 samples. It is not recommended to modify the NRSMPL.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply