ADC Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Interrupt

1,849件の閲覧回数
Rwaghmare
Contributor I

Hi Everyone,

I have configured ADC interrupt and also written ISR for respective interrupt. My interrupt is getting triggered on every ADC value change. Can anyone help me in following :

How to use Hardware compare function?

Which values should we compare?

 

0 件の賞賛
返信
1 返信

1,843件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

please refer to chapter 44.5.5 Automatic compare function of the RM.
As mentioned there the compare mode is determined by SC2[ACFGT], SC2[ACREN] bits, and the values in the Compare Value registers (CV1 and CV2). After the input is sampled and converted, the compare values in CV1 and CV2 are used as described in the table 44-5. If the condition selected evaluates true, SC1n[COCO] is set.

Upon completion of a conversion while the compare function is enabled, if the compare condition is not true, SC1n[COCO] is not set and the conversion result data will not be transferred to the result register, Rn.

BR, Petr

0 件の賞賛
返信