32K148 Programming Issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

32K148 Programming Issues

621件の閲覧回数
gary_yang
Contributor II

Dear Sir:

S32K148 address 0x400~0x40F programmed the following data.

gary_yang_0-1751507261155.pnggary_yang_0-1751507261155.png

 

After programming successfully, can the SWD interface be used to read the flash content or reprogram it?

0 件の賞賛
返信
1 返信

610件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi gary,

There is a detailed introduction to the Flash configuration area of ​​the S32K1xx series MCU (Flash configuration filed 0x400~0x40F): S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解 里有详细的介绍

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信