yocto project build failure based on SDK BSP44

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto project build failure based on SDK BSP44

409件の閲覧回数
hittzt
Senior Contributor I

Hi,

 

I noticed that the SDK BSP44 has been released, and I tried to build the yocto project following the BSP44 reference user manual. But it failed due to no NXP-EULA license file. And I tried to find the file from the flexra download site, and I did not find it.

So would you please help to check the issue, or where can I get the license file to build the project?

 

Thanks,

Zhantao

0 件の賞賛
返信
3 返答(返信)

377件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,hittzt

Thank you for contacting us.

Are you using RDB2 or RDB3? Could you share more error information for us?

BR

Joey 

0 件の賞賛
返信

373件の閲覧回数
hittzt
Senior Contributor I

Yes, I use RDB3 for test, and the build errors are like:

sources/meta-alb/meta-alb-bsp/recipes-bsp/ddr-firmware/ddr-firmware.bb: Unable to get checksum for ddr-firmware SRC_URI entry NXP-EULA: file could not be found
The following paths were searched:
${NXP_FIRMWARE_LOCAL_DIR}/fsl-auto/NXP-EULA
sources/meta-alb/meta-alb-bsp/recipes-bsp/ddr-firmware/ddr-firmware-1.0/fsl-auto/NXP-EULA
sources/meta-alb/meta-alb-bsp/recipes-bsp/ddr-firmware/ddr-firmware/fsl-auto/NXP-EULA
sources/meta-alb/meta-alb-bsp/recipes-bsp/ddr-firmware/files/fsl-auto/NXP-EULA

......

The NXP-EULA is a new license of NXP? Where can I get it to make the yocto project build pass?

 

Thanks,

Zhantao

0 件の賞賛
返信

351件の閲覧回数
Joey_z
NXP Employee
NXP Employee

hi,hittzt

NXP-EULA can be downloaded here and placed in the above path.

Joey_z_0-1750849583292.png

Hope it can help you.

BR

Joey

 

0 件の賞賛
返信