what's the meaning and usage of life cycle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what's the meaning and usage of life cycle

Jump to solution
891 Views
brian_w
Contributor III

Hi,

In the S32G2 RM, there is "life cycle". What's the full meaning of life cycle, and how should we use it?

0 Kudos
Reply
1 Solution
877 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The "life cycle" under the S32G2 RM refers to the stage of the application being developed. As seen in the S32G2 RM [Page 1142, S32G2 Reference Manual, Rev. 6, 11/2022]:

"Life cycle state (blocks some boot modes that are valid only for specific life cycle states)"

Also:

DanielAguirre_0-1682107845750.png

Which provides the SW state of development to the platform.

At the end, this feature should be related to the HSE_H:

DanielAguirre_1-1682107924649.png

If more information is required, HSE is under NDA and confidential, for which we recommend sending this inquiry to your local NXP representative/FAE to start the process on this topic.

Please, let us know.

View solution in original post

1 Reply
878 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The "life cycle" under the S32G2 RM refers to the stage of the application being developed. As seen in the S32G2 RM [Page 1142, S32G2 Reference Manual, Rev. 6, 11/2022]:

"Life cycle state (blocks some boot modes that are valid only for specific life cycle states)"

Also:

DanielAguirre_0-1682107845750.png

Which provides the SW state of development to the platform.

At the end, this feature should be related to the HSE_H:

DanielAguirre_1-1682107924649.png

If more information is required, HSE is under NDA and confidential, for which we recommend sending this inquiry to your local NXP representative/FAE to start the process on this topic.

Please, let us know.