using configtool on S32 Design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using configtool on S32 Design studio

1,477 Views
sangrael
Contributor I

Hi NXP,

 

I am just trying to configure all comms and GPIOs on S32G274A chip using configtool on S32 Design studio.

 

It says MCU is not selected. 

 

Could you help me out?

 

Regards,

Sangrae

0 Kudos
Reply
3 Replies

189 Views
Petro
Contributor I

Same problem with S32K144. The project is created, compiled, and loaded, but ConfigTool it doesn't see the processor target.

0 Kudos
Reply

1,467 Views
asap
NXP Employee
NXP Employee

Hi Sangrae,

You could open S32DS (ver3.4 or later), create a S32DS application project->select the right core you are using -> add the SDK(RTD) for each of the core (if you are using M7). if RTD not yet installed, please install RTD to S32DS also. 

You could refer to the S32G training hub (S32G2 Technical overview) for more detail guide. 

Albert
0 Kudos
Reply

159 Views
Petro
Contributor I

Where can I get an RTD? It's not in the extension list.

0 Kudos
Reply