using configtool on S32 Design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using configtool on S32 Design studio

1,352件の閲覧回数
sangrael
Contributor I

Hi NXP,

 

I am just trying to configure all comms and GPIOs on S32G274A chip using configtool on S32 Design studio.

 

It says MCU is not selected. 

 

Could you help me out?

 

Regards,

Sangrae

0 件の賞賛
返信
3 返答(返信)

64件の閲覧回数
Petro
Contributor I

Same problem with S32K144. The project is created, compiled, and loaded, but ConfigTool it doesn't see the processor target.

0 件の賞賛
返信

1,342件の閲覧回数
asap
NXP Employee
NXP Employee

Hi Sangrae,

You could open S32DS (ver3.4 or later), create a S32DS application project->select the right core you are using -> add the SDK(RTD) for each of the core (if you are using M7). if RTD not yet installed, please install RTD to S32DS also. 

You could refer to the S32G training hub (S32G2 Technical overview) for more detail guide. 

Albert
0 件の賞賛
返信

34件の閲覧回数
Petro
Contributor I

Where can I get an RTD? It's not in the extension list.

0 件の賞賛
返信