source.codeaurora.org is unavailable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

source.codeaurora.org is unavailable

ソリューションへジャンプ
2,883件の閲覧回数
jiahaisheng
Contributor I

I am in the github codebase:

https://github.com/nxp-auto-linux/ipc-shm-us/tree/release/SW32R45_IPCF_4.4.0_D2303

To download the code for /ipc-shm-us/common/,

use the command: git submodule update --init --recursive

will indicate fatal: unable to access 'https://source.codeaurora.org/external/autobsps32/ipcf/ipc-shm/': Could not resolve host: source.codeaurora.org,

how do I get the code under ipc-shm-us/common/?

Thanks!

0 件の賞賛
返信
1 解決策
2,792件の閲覧回数
nxf92108
NXP Employee
NXP Employee

Hi,

Yes, ipc-shm-us/common is the code from ipc-shm/.

Please, let us know.

元の投稿で解決策を見る

2 返答(返信)
2,876件の閲覧回数
jiahaisheng
Contributor I

Or is the code under ipc-shm-us /common/ the code under ipc-shm/?

0 件の賞賛
返信
2,793件の閲覧回数
nxf92108
NXP Employee
NXP Employee

Hi,

Yes, ipc-shm-us/common is the code from ipc-shm/.

Please, let us know.