source.codeaurora.org is closed, where is the nxp source code? how to search in new address?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

source.codeaurora.org is closed, where is the nxp source code? how to search in new address?

ソリューションへジャンプ
1,357件の閲覧回数
hulk101
Contributor III

source.codeaurora.org is closed, where is the nxp source code? how to search in new address?  I am using linux bsp 32.0 user manual for s32g2 platforms.

S32G-VNP-RDB2 

0 件の賞賛
返信
1 解決策
1,331件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hulk101 

Thanks for you reply.

For example, when you want to access the Linux source code, the URL from your documents would be https://source.codeaurora.org/external/autobsps32/linux , currently, it could be https://github.com/nxp-auto-linux/linux

If possible, I suggest using newer BSP version, which may be with more bug fixes and new features.

 

BR

Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,332件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hulk101 

Thanks for you reply.

For example, when you want to access the Linux source code, the URL from your documents would be https://source.codeaurora.org/external/autobsps32/linux , currently, it could be https://github.com/nxp-auto-linux/linux

If possible, I suggest using newer BSP version, which may be with more bug fixes and new features.

 

BR

Chenyin

0 件の賞賛
返信
1,345件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hulk101 

Thanks for your post.

Yes, the older BSP is deployed on codeaurora, since it is closed, the newer version source code could not be found via https://github.com/orgs/nxp-auto-linux/repositories?type=all

You may check correct repo according to the requirements.

 

BR

Chenyin

0 件の賞賛
返信
1,344件の閲覧回数
hulk101
Contributor III
Thankyou,
Could you please help me find the newer version of the source code? The document's that I'm referring to are showing the same repo's.
0 件の賞賛
返信