s32g274a uart is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32g274a uart is not working

1,725 次查看
kevin_Tai
Contributor I

Hi All,

I have some problem with S32G UART 

1. The environment :

board: S32G274A EVB

os: Linux s32g274aevb 5.4.69

2. The Muxed Function between uart pin and gpio pin

LINFlexD_0:  TX: PC09  RX: PC10

LINFlexD_1:  TX: PC08  RX: PC04

LINFlexD_2:  TX: PK11  RX: PK12

We can see three uart devices ttyLF0, ttyLF1 and ttLF2. But only ttyLF0 is working OK,  ttyLF1 and ttyLF2 are not . 

root@s32g274aevb:~# ls /dev/ttyLF*
/dev/ttyLF0 /dev/ttyLF1 /dev/ttyLF2

I had checked and configured the device tree of uart in the kernel. Is there anything that needs to be modified besides the device tree?

0 项奖励
回复
1 回复

1,591 次查看
vimalrajendran
Contributor II

Hi ,

          i am also facing same problem with ttyLF1 port

0 项奖励
回复