s32g-vnp-rdb2 debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32g-vnp-rdb2 debugger

ソリューションへジャンプ
3,303件の閲覧回数
skseofh
Contributor II

Hi

I'm using S32G-VNP-RDB2.

 

I know that there are two debugger(T32 and S32 Debugger) to debug S32G274A.

 

I have PE micro multi-link debugger.

PE micro is supported to debug S32G274A?

0 件の賞賛
返信
1 解決策
3,292件の閲覧回数
bpe
NXP Employee
NXP Employee

You have to consult at your debug probe vendor, PE Micro, for the list of
supported debug targets and availability of the corresponding plugins.
S32DS does support PE Micro probes in general, provided that the appropriate
plugin is installed. You should be able to do basic debug with it, but certain
features, e.g. trace, may not be available.

Best Regards,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,293件の閲覧回数
bpe
NXP Employee
NXP Employee

You have to consult at your debug probe vendor, PE Micro, for the list of
supported debug targets and availability of the corresponding plugins.
S32DS does support PE Micro probes in general, provided that the appropriate
plugin is installed. You should be able to do basic debug with it, but certain
features, e.g. trace, may not be available.

Best Regards,
Platon

 

0 件の賞賛
返信
2,972件の閲覧回数
murphy_xie
Contributor I

Hi NXP

      when i try to debug s32g274A,I can`t find the S32G family.However I can find K1 and K3 is anything wrong?

tks.

0 件の賞賛
返信