s32g smp support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,482件の閲覧回数
Jason_leee
Contributor I

Could someone give me some information or reference about s32g274a smp? thanks very much.

タグ(1)
0 件の賞賛
返信
1 解決策
4,423件の閲覧回数
bpe
NXP Employee
NXP Employee

S32G274 M7 cores are primarily targeted at simple tasks. They are not well-equipped for SMP. Although it is theoretically possible to use them for SMP, there are no ready solutions or recommendations for that. Our suggestion in this regard is, consider developing your SMP application in a supported way, namely in an SMP-enabled OS environment running on A53 cores.

Best Regards,
Platon

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,442件の閲覧回数
Jason_leee
Contributor I

Thanks for your reply. I want use smp function on s32g274a M7 cluster, could you give me some reference?

Best regards.

Jason

0 件の賞賛
返信
4,424件の閲覧回数
bpe
NXP Employee
NXP Employee

S32G274 M7 cores are primarily targeted at simple tasks. They are not well-equipped for SMP. Although it is theoretically possible to use them for SMP, there are no ready solutions or recommendations for that. Our suggestion in this regard is, consider developing your SMP application in a supported way, namely in an SMP-enabled OS environment running on A53 cores.

Best Regards,
Platon

 

 

0 件の賞賛
返信
4,417件の閲覧回数
Jason_leee
Contributor I

Okay, thanks a lot. it seems that i need to find a workaroud solution.

Best Regards,

Jason

0 件の賞賛
返信
4,450件の閲覧回数
bpe
NXP Employee
NXP Employee


The recommended approach to SMP on S32G274 processors is to run a general purpose,
SMP-enabled OS on it's A53 core cluster. Available form NXP is a Linux-centric
Automotive BSP which has SMP enabled by default. More information can be found
in Automotive BSP User Manual.

 

Hope this Helps,
Platon

0 件の賞賛
返信