s32g emmc hs200 in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32g emmc hs200 in linux

852 Views
shiyiheng
Contributor III

May I ask how to configure HS200 on s32G linux? Under uboot, it can be done by modifying Kconfig, but I couldn't find a place to configure it on linux?

0 Kudos
Reply
3 Replies

842 Views
Joey_z
NXP Employee
NXP Employee

hi,shiyiheng

Thank you for your information.

Which version of BSP are you using? And are you using RDB2 or RDB3?

BR

Joey

0 Kudos
Reply

837 Views
shiyiheng
Contributor III

The rdb3 board I'm using is currently based on BSP34 and I plan to upgrade to bsp39. However, I haven't found a way to configure hs200 under either version of linux. The default is hs400es.

0 Kudos
Reply

828 Views
Joey_z
NXP Employee
NXP Employee

hi,shiyiheng

Thank you for your information.

You can refer to the AN13667(AN13667: eMMC Enablement and Debugging Tips Application Note) and S32G2_LinuxBSP_41.0_User_Manual.pdf to find some information about using HS200 in Linux.

Joey_z_0-1751601084672.pngJoey_z_0-1751601084672.pngJoey_z_1-1751601104580.pngJoey_z_1-1751601104580.png

Hope it can help you.

BR

Joey

0 Kudos
Reply