read write in NOR flash from BL2 level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

read write in NOR flash from BL2 level

3,932 Views
Jayashree
Contributor II

I am working on S32G3 (Yocto BSP 43) and trying to log secure-boot (BL2) errors into QSPI NOR.

I tried to use the MMIO read/write APIs from BL2; however, the boot process appears to halt immediately after the API call.

Jayashree_0-1767962938834.png

 


I attempted to use xspi_read() / xspi_write() APIs, but BL2 build fails with undefined reference errors. On inspection, these APIs are not implemented in ATF; same with  FSPI read/write APIs


Could you please confirm whether read/write access from BL2 is supported when secure boot is enabled? If it is supported, could you advise which APIs are recommended for this use case? Alternatively, I would appreciate your guidance on feasible approaches or recommended alternatives for logging or data persistence from BL2.


Best regards,
Jayashree

 

 

0 Kudos
Reply
11 Replies

3,897 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Jayashree,

Thanks for contacting us again, it is always great to support you. Regarding your question, I have not seen any similar implementation in the past, however, here are my recommendatins:

to use xspi_read/xspi_write you need to include:

#include <drivers/nxp/flexspi/fspi_api.h>

in your source file, I was able to add xspi_write into bl2_main() and build. Note that I only tested the build process.

You could also use io_read/io_write as done in bl_common.c#L94.

 

When you mentioned the MMIO read/write, do you mean the functions in include/lib/mmio.h?

 

Let me know if this helps

 

0 Kudos
Reply

3,763 Views
Jayashree
Contributor II

Thank you for the quick response. As per your suggestion, I have included the recommended header file and attempted to call the XSPI APIs in the bl2_main.c file. However, I am still encountering an undefined reference/ symbol error during the build.

 
 

Jayashree_2-1768308318568.png

 

For your reference, I have attached the modified file below. I would appreciate it if you could please review it and let me know if I am missing any required configuration or build changes.

/*
* Copyright (c) 2013-2023, Arm Limited and Contributors.
*
* SPDX-License-Identifier: BSD-3-Clause
*/

#include <assert.h>
#include <stdint.h>

#include <arch_helpers.h>
#include <arch_features.h>
#include <bl1/bl1.h>
#include <bl2/bl2.h>
#include <common/bl_common.h>
#include <common/debug.h>
#include <drivers/auth/auth_mod.h>
#include <drivers/auth/crypto_mod.h>
#include <drivers/console.h>
#include <drivers/fwu/fwu.h>
#include <drivers/nxp/flexspi/fspi_api.h>
#include <lib/bootmarker_capture.h>
#include <lib/extensions/pauth.h>
#include <lib/pmf/pmf.h>
#include <plat/common/platform.h>

#include "bl2_private.h"

#ifdef __aarch64__
#define NEXT_IMAGE "BL31"
#else
#define NEXT_IMAGE "BL32"
#endif

/* ================= NOR TEST CONFIG ================= */
#define NOR_TEST_OFFSET 0x400U
#define NOR_TEST_SIZE 4U
/* ================================================== */

#if ENABLE_RUNTIME_INSTRUMENTATION
PMF_REGISTER_SERVICE(bl_svc, PMF_RT_INSTR_SVC_ID,
BL_TOTAL_IDS, PMF_DUMP_ENABLE);
#endif

#if RESET_TO_BL2
/*******************************************************************************
* Setup function for BL2 when RESET_TO_BL2=1
******************************************************************************/
void bl2_el3_setup(u_register_t arg0, u_register_t arg1, u_register_t arg2,
u_register_t arg3)
{
/* Perform early platform-specific setup */
bl2_el3_early_platform_setup(arg0, arg1, arg2, arg3);

/* Perform late platform-specific setup */
bl2_el3_plat_arch_setup();

#if CTX_INCLUDE_PAUTH_REGS
/*
* Assert that the ARMv8.3-PAuth registers are present or an access
* fault will be triggered when they are being saved or restored.
*/
assert(is_armv8_3_pauth_present());
#endif /* CTX_INCLUDE_PAUTH_REGS */
}
#else /* RESET_TO_BL2 */

/*******************************************************************************
* Setup function for BL2 when RESET_TO_BL2=0
******************************************************************************/
void bl2_setup(u_register_t arg0, u_register_t arg1, u_register_t arg2,
u_register_t arg3)
{
/* Perform early platform-specific setup */
bl2_early_platform_setup2(arg0, arg1, arg2, arg3);

/* Perform late platform-specific setup */
bl2_plat_arch_setup();

#if CTX_INCLUDE_PAUTH_REGS
/*
* Assert that the ARMv8.3-PAuth registers are present or an access
* fault will be triggered when they are being saved or restored.
*/
assert(is_armv8_3_pauth_present());
#endif /* CTX_INCLUDE_PAUTH_REGS */
}
#endif /* RESET_TO_BL2 */

/*******************************************************************************
* The only thing to do in BL2 is to load further images and pass control to
* next BL. The memory occupied by BL2 will be reclaimed by BL3x stages. BL2
* runs entirely in S-EL1.
******************************************************************************/
void bl2_main(void)
{
entry_point_info_t *next_bl_ep_info;
uint32_t write_val = 0xA5A5A5A5;
uint32_t read_val = 0;
int rc;

#if ENABLE_RUNTIME_INSTRUMENTATION
PMF_CAPTURE_TIMESTAMP(bl_svc, BL2_ENTRY, PMF_CACHE_MAINT);
#endif

NOTICE("BL2: %s\n", version_string);
NOTICE("BL2: %s\n", build_message);

/* Perform remaining generic architectural setup in S-EL1 */
bl2_arch_setup();

#if PSA_FWU_SUPPORT
fwu_init();
#endif /* PSA_FWU_SUPPORT */

crypto_mod_init();

/* Initialize authentication module */
auth_mod_init();

/* Initialize the Measured Boot backend */
bl2_plat_mboot_init();

/* Initialize boot source */
bl2_plat_preload_setup();

/* ============================================================
* XSPI / NOR DIRECT ACCESS TEST (PERSISTENT LOGGING EXPERIMENT)
* ============================================================ */
NOTICE("\n===============================================\n");
NOTICE("BL2: XSPI NOR direct access test\n");
NOTICE("BL2: NOR offset = 0x%x\n", NOR_TEST_OFFSET);
NOTICE("===============================================\n");

NOTICE("BL2: Writing 0x%08x to NOR\n", write_val);
rc = xspi_write(NOR_TEST_OFFSET, &write_val, sizeof(write_val));
if (rc != 0) {
ERROR("BL2: xspi_write FAILED (%d)\n", rc);
} else {
NOTICE("BL2: xspi_write OK\n");
}

NOTICE("BL2: Reading back from NOR\n");
rc = xspi_read(NOR_TEST_OFFSET, &read_val, sizeof(read_val));
if (rc != 0) {
ERROR("BL2: xspi_read FAILED (%d)\n", rc);
} else {
NOTICE("BL2: xspi_read OK, value = 0x%08x\n", read_val);
}

NOTICE("===============================================\n");
NOTICE("BL2: XSPI NOR test done, continuing boot\n");
NOTICE("===============================================\n\n");

/* Load the subsequent bootloader images. */
next_bl_ep_info = bl2_load_images();

/* Teardown the Measured Boot backend */
bl2_plat_mboot_finish();

#if !BL2_RUNS_AT_EL3
#ifndef __aarch64__
/*
* For AArch32 state BL1 and BL2 share the MMU setup.
* Given that BL2 does not map BL1 regions, MMU needs
* to be disabled in order to go back to BL1.
*/
disable_mmu_icache_secure();
#endif /* !__aarch64__ */

#if ENABLE_PAUTH
/*
* Disable pointer authentication before running next boot image
*/
pauth_disable_el1();
#endif /* ENABLE_PAUTH */

#if ENABLE_RUNTIME_INSTRUMENTATION
PMF_CAPTURE_TIMESTAMP(bl_svc, BL2_EXIT, PMF_CACHE_MAINT);
#endif

console_flush();

/*
* Run next BL image via an SMC to BL1. Information on how to pass
* control to the BL32 (if present) and BL33 software images will
* be passed to next BL image as an argument.
*/
smc(BL1_SMC_RUN_IMAGE, (unsigned long)next_bl_ep_info, 0, 0, 0, 0, 0, 0);
#else /* if BL2_RUNS_AT_EL3 */

NOTICE("BL2: Booting " NEXT_IMAGE "\n");
print_entry_point_info(next_bl_ep_info);

#if ENABLE_RUNTIME_INSTRUMENTATION
PMF_CAPTURE_TIMESTAMP(bl_svc, BL2_EXIT, PMF_CACHE_MAINT);
#endif

console_flush();

#if ENABLE_PAUTH
/*
* Disable pointer authentication before running next boot image
*/
pauth_disable_el3();
#endif /* ENABLE_PAUTH */

bl2_run_next_image(next_bl_ep_info);
#endif /* BL2_RUNS_AT_EL3 */
}

0 Kudos
Reply

3,710 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Jayashree,

I am sorry, I might have been compiling an unsaved version of the file, I retried now and I as not able to compile it, and after many attempts I was not able to do it. For now I have only two recommendations, either try to use io_read/io_writ as I mentioned in my first reply or use the recently added demo project using RTD on the A53 core as base to port the SPI driver to ATF.

To access the second one, log into FlexNet and Follow this path:

Automotive SW – S32G Reference Software > Automotive SW – S32G RTD on A53 > RTD_ON_S32G A53_0.1.0 Solution demo

If you are not able to see one of the options, log into flex net and use this link.

Please note that this is only a recommendations and none were tested on my side, both may come with unrecoverable issues, being that ATF is a very early stage of booting for the A53 cores.

 

Sorry for the inconveniences.

0 Kudos
Reply

3,309 Views
Jayashree
Contributor II

Hello,

Thank you for your response.

I tried using the io_read/io_write APIs as suggested earlier. While the code built successfully,
i was not able to write or seek (refer image below)

io.png 

Regarding the second approach, I was not able to proceed with the RTD demo on the A53 core. Instead, I attempted an alternative approach by porting the SPI/NOR access APIs from U-Boot into the BL2 stage. I was able to resolve the build issues and generate the binaries successfully; however, the boot process halts as soon as the SPI API is invoked from BL2.

flexspi_port.png

 

At this point, I wanted to check if there are any other recommended or supported alternatives to log or persist minimal data at the BL2 stage that can later be accessed from Linux. Specifically, is there any safe mechanism or reference design for early-boot logging on S32G, or is BL2 fundamentally not suitable for such use cases?

I understand and acknowledge that BL2/ATF is a very early boot stage and that such changes may introduce unrecoverable issues, but any guidance or best practices from your experience would be very helpful.

Thank you

0 Kudos
Reply

3,291 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Jayashree,

I tried searching other options to possibly overcome the problem, however, I was not able to find any reference on how to achieve this. As you are aware, since ATF is very early in the boot process reaching the flash memory is out of its scope. As a personal recommendation, the earliest log I can think of i from u-boot, you could use the ext4write, for which you will need to add the following configuration in your .config file:

CONFIG_CMD_EXT4_WRITE=y

You can check more about the ext4 operations in https://docs.u-boot.org/en/latest/usage/filesystems/ext4.html.

With this commands you can write into a file in the Linux filesystem.

 

I hope this helps

0 Kudos
Reply

3,226 Views
Jayashree
Contributor II

Hello,

Thank you for the clarification and for confirming the limitations of ATF/BL2 with respect to flash access.

I am still exploring whether it is technically possible to perform minimal read/write operations directly from BL2 itself. I understand this is outside the typical scope, but I wanted to check feasibility. Specifically, I was wondering if accessing eMMC from BL2 could be possible by explicitly adding the required MMC dependencies. While reviewing the codebase, I noticed that mmc.c already defines block-level read and write APIs. Would it be possible to initialize the MMC subsystem early enough in BL2 and use these block read/write functions for minimal logging purposes?

I fully understand the risks involved and I wanted to confirm whether this approach is fundamentally unsupported or simply not recommended.

Thank you for the support.
Best regards,
Jayashree

0 Kudos
Reply

3,189 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Jayashree,

It is possible in theory, if you initialized all the required clocks and modules, but I cannot guide much guidance. You could use the Usdhc_Ip_example_S32G399A_M7 sample project to know how to configure and access the SD card. Please note that you must ensure not to interfere with the partitions needed by Linux, if you decide to take this approach I would recommend reserving part of the memory for the log purpose and not use it for anything else.

 

Best regards.

0 Kudos
Reply

3,108 Views
Jayashree
Contributor II

Hello @alejandro_e,

I’m pleased to share that I am now able to write to eMMC from BL2. As a next step, I would like to log timestamps along with the data. I came across the Performance Measurement Framework (PMF), but I am unsure how to enable and use it at this stage and what macros flags should be enabled to access this feature.

Could you please provide some guidance on how to proceed?

0 Kudos
Reply

3,097 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Jayashree,

Since the PMF is not provided by ARM and not by NXP I cannot give you much support. However, I would recommend checking the ARM documentation that module https://trustedfirmware-a.readthedocs.io/en/latest/perf/psci-performance-instr.html  

0 Kudos
Reply

3,087 Views
Jayashree
Contributor II

Hello @alejandro_e,

Thank you for your response.

I believe the link shared refers to PSCI performance instrumentation, which appears to be different from the general Performance Measurement Framework (PMF) used for timestamp collection in TF-A.

https://github.com/nxp-auto-linux/arm-trusted-firmware/blob/c834244b9c54c79e80315aecc9807f5b0eb79342...


From the TF-A documentation, PMF seems to be a generic framework that relies on the system counter and can be enabled via build flags:

Since PMF is part of TF-A itself, could you please recheck whether it is truly unsupported on the S32G platform?

Thank you.

0 Kudos
Reply

3,079 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Jayashree,

Thanks for the clarification. Regarding the support, the PMF library may or may not run correctly, however I was not able to find any reference for it in our documentation, so you will need to test it yourself and we won't be able to give you much guidance or support on that topic.

I apologize for the inconveniences.

0 Kudos
Reply