Hi,NXP
I'm testing the S32G with rdb2 hardware, I haven't found a M core pfe master program that I can run on qspi, I just want the M core to be able to send out udp data via pfe just fine, is there a routine for that?
BR.
Hello, @youke
Thanks for your feedback
You mean that the PFE master with LWIP project works fine from your side via debugger, but failed for QSPI boot when flashed to the QSPI?
May I know which CMM file you used to test the elf file? and share the steps for generating blob image from raw binary.
BR
Chenyin
Hello, @youke
Thanks for your reply.
May I know if it is possible to share the elf/raw binary/linker file used? I would help to check it.
If it is not convenient to share it in this public community, please tell me and I could help to create private sessions.
BR
Chenyin
Hi, chenyin
I haven't made any corresponding modifications to the initialization code; I only commented out some unused functions in the main function.
These are the QSPI-related parameters in IVT. Could they have an impact?
What other modifications do I need to make?
BR.
Hello, @youke
Thanks for your post.
Since UDP is based on IP protocol, for sending UDP packet via PFE from M core's perspective, you need to combine the PFE driver and IP stack together(for example, LWIP), I suggest referencing the demo that mentioned from example_application directory of the PFE MCAL for details.
BR
Chenyin
BR
Chenyin
Hi,chenyin
I have tested this routine, I now want to simply run through the ping test, I tested the cmm debugging and it works, but I can't get it to start after I flushed it to QSPI, do you have a pfe master routine available for qspi?
BR.