pfeng: Version magic is inconsistent

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pfeng: Version magic is inconsistent

1,517件の閲覧回数
972276616
Contributor II

Hi,

I used menuconig to change PREEMPT_RT to y, i.e

The Preemption Model is Fully Preemptible Kernel (real-time). After compiling and booting the kernel, the boot log displays:

[ 1.504617] pfeng: version magic '5.10.90-rt60+g47a49b91d4d4 SMP preempt mod_ unload aarch64' should be '5.10.90-rt60+g47a49b91d4d4 SMP preempt_rt mod_unload aarch64'
[ 1.756999] sja1110: version magic '5.10.90-rt60+g47a49b91d4d4 SMP preempt mo d_unload aarch64' should be '5.10.90-rt60+g47a49b91d4d4 SMP preempt_rt mod_unloa d aarch64'
[ 1.757136] sja1110: version magic '5.10.90-rt60+g47a49b91d4d4 SMP preempt mo d_unload aarch64' should be '5.10.90-rt60+g47a49b91d4d4 SMP preempt_rt mod_unloa d aarch64'

 

Symptom NIC PFE2 cannot be identified after the system starts.

How should I modify to normally identify the network card device PFE?

タグ(2)
0 件の賞賛
返信
1 返信

1,508件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The kernel you are using is not part of the S32G standard bsp so please use the standard bsp that is not tested with PREEMP_RT.

 

Regards

0 件の賞賛
返信