how to add UART m7 example code in M7-Sample bootloader code.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to add UART m7 example code in M7-Sample bootloader code.

2,755 次查看
uiv12187
Contributor I

Hello,

when we are setting boot target as m7 that same time when m7 booting that time i want to print m7 bootloader is up string in UART serial port prompt. how to do this can you please help me to complete this task

0 项奖励
回复
5 回复数

2,673 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @uiv12187 

Thanks for your reply.

I feel sorry that the bootloader included in GoldVIP only supports the EB, while there is no S32DS version.

I do apologize.

 

BR

Chenyin

0 项奖励
回复

2,719 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @uiv12187 

Thanks for your reply

I could understand your requirement, the code you mentioned is relatively old and simple, for M core bootloader, I could suggest directly using bootloader project from GoldVIP, while the UART is by default supported.

You may try it from the following link:

https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER

chenyin_h_0-1728639014643.pngchenyin_h_0-1728639014643.png

 

 

BR
Chenyin

0 项奖励
回复

2,685 次查看
uiv12187
Contributor I

Hello,

 

Thank you for the message.

bootloader example looks like created for EB tresos Studio, but I need examples for s32 design studio can you please help me on this.

 

Regards,

Raghavendra

0 项奖励
回复

2,728 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @uiv12187 

Thanks for your post.

May I know if you are working with S32G3 or G2?

Also would you help to share where you get the sample bootloader, which software package is the bootloader from?

Thanks

 

BR
Chenyin

0 项奖励
回复

2,723 次查看
uiv12187
Contributor I

Hello Chenyin,

Thank you for the response,

-> I am working with S32G3.

-> bellow i copied sample bootloader link i used for configuring m7 as boot target and also i want to marge m7 UART code into this bootloader code.

GitHub - nxp-auto-linux/m7-sample at release/bsp38.0

 

Thanks

BR

Raghavendra

0 项奖励
回复