ethtool --cable-test trx6 report error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ethtool --cable-test trx6 report error

5,842 Views
liujialu_2024
Contributor III

on the board of S32G-VNP-RDB2, check the cable "100Base-T1 TRX6". 

The cable links well, and ping woks well, but cable-test report error:

root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Unknown


root@s32g274ardb2:~# ./mdio pfeng-emac-2 mmd 0x0a:01 raw 0x8330
0x2007

0x2007 means: Unable to detect. then why?

liujialu_2024_0-1765960182064.png


test cable open is OK

root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Open Circuit


root@s32g274ardb2:~# ./mdio pfeng-emac-2 mmd 0x0a:01 raw 0x8330
0x2002

test cable short is OK

root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Short within Pair


root@s32g274ardb2:~# ./mdio pfeng-emac-2 mmd 0x0a:01 raw 0x8330
0x2001

 

0 Kudos
Reply
13 Replies

5,628 Views
liujialu_2024
Contributor III

About "Pair A code Unknown",

google AI answers:

Common Causes:

Active Link: Performing the test while the Ethernet is plugged into a powered-on gigabit switch can interfere with results; it is often recommended to not be on an active link for TDR mode.

and from "um549820-UM11107 Software User Manual for SJA1110(2.0).pdf"

6.9.2 Cable test and TDR

the PHY can detect open and short circuits between the twisted-pair lines when neither of the link partners is transmitting.

Does the cable-test require connection but not activation?

Actually, trx6 linked with t1-converter, it's "Pair A code OK" when the converter's link LED not bling-bling.

On the contrary, when the LED bling-bling, it's "Pair A code Unknown"。

@Joey_z Please help confirm. Thank you.

0 Kudos
Reply

5,617 Views
liujialu_2024
Contributor III
but when trx6 in master mode.
$ ethtool -s trx6 master-slave forced-master
it always report "Pair A code OK", Whether the converter's LED bling-bling or not
0 Kudos
Reply

5,614 Views
Joey_z
NXP Employee
NXP Employee

hi,liujialu

When you set the ethtool -s trx6 master-slave forced-master.

I think the converter should be set to slave. the LED of T1 will bling-bling using the ethtool --cable-test trx6.

BR

Joey

0 Kudos
Reply

5,620 Views
Joey_z
NXP Employee
NXP Employee

hi,liujialu_2024

Thank you for your reply.

I have helped you to test the slave mode of trx6.

root@s32g274ardb2:~# ip link set dev trx6 up
root@s32g274ardb2:~# ethtool -s trx6 master-slave forced-slave
root@s32g274ardb2:~# ethtool --cable-test trx6         //converter set to the Master
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code OK
root@s32g274ardb2:~# ethtool --cable-test trx6   //converter set to the slave
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code OK

The T1 LED still is bling-bling when I use the commend of ethtool --cable-test trx6. We do not use the same converter device.

BR

Joey

0 Kudos
Reply

5,744 Views
Joey_z
NXP Employee
NXP Employee

hi,liujialu_2024

Thank you for your information and reply.

I use the default BS42 for this testing.

This is the test result for trx6.

root@s32g274ardb2:~# dmesg | grep -i "sja"
[ 0.828889] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 0.834314] sja1105 spi5.1: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 0.851072] sja1105 spi5.1: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 4.876989] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 4.882428] sja1105 spi5.1: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 4.899197] sja1105 spi5.1: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 5.053247] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 5.058672] sja1105 spi5.1: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 5.075441] sja1105 spi5.1: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 5.092543] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 5.097958] sja1105 spi5.1: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 5.114723] sja1105 spi5.1: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 7.103854] sja1110: loading out-of-tree module taints kernel.
[ 7.117294] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[ 7.124319] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[ 9.153856] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 9.159387] sja1105 spi5.1: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 9.181619] sja1105 spi5.1: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 9.430825] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 9.438127] sja1105 spi5.1: Port 2 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 9.454444] sja1105 spi5.1: Port 3 interpreting RGMII delay settings based on "phy-mode" property, please update device tree to specify "rx-internal-delay-ps" and "tx-internal-delay-ps"
[ 9.732411] sja1105 spi5.1: configuring for fixed/2500base-x link mode
[ 9.741123] sja1105 spi5.1: Link is Up - 2.5Gbps/Full - flow control off
[ 9.808065] sja1105 spi5.1 p1 (uninitialized): PHY [spi5.1-base-tx:01] driver [NXP CBTX (SJA1110)] (irq=POLL)
[ 9.856358] sja1105 spi5.1 trx5 (uninitialized): PHY [spi5.1-base-t1:01] driver [NXP C45 TJA1103] (irq=POLL)
[ 9.934013] sja1105 spi5.1 trx6 (uninitialized): PHY [spi5.1-base-t1:02] driver [NXP C45 TJA1103] (irq=POLL)
[ 10.011587] sja1105 spi5.1 trx7 (uninitialized): PHY [spi5.1-base-t1:03] driver [NXP C45 TJA1103] (irq=POLL)
[ 10.049845] sja1105 spi5.1 trx8 (uninitialized): PHY [spi5.1-base-t1:04] driver [NXP C45 TJA1103] (irq=POLL)
[ 10.085888] sja1105 spi5.1 trx9 (uninitialized): PHY [spi5.1-base-t1:05] driver [NXP C45 TJA1103] (irq=POLL)
[ 10.116363] sja1105 spi5.1 trx10 (uninitialized): PHY [spi5.1-base-t1:06] driver [NXP C45 TJA1103] (irq=POLL)
[ 592.917267] sja1105 spi5.1 trx5: configuring for phy/internal link mode
[ 772.869305] sja1105 spi5.1 trx6: configuring for phy/internal link mode
[ 1143.821448] sja1105 spi5.1 p1: configuring for phy/internal link mode
[ 1145.880585] sja1105 spi5.1 p1: Link is Up - 100Mbps/Full - flow control off
[ 1224.413285] sja1105 spi5.1 p2: configuring for fixed/rgmii-txid link mode
[ 1224.418540] sja1105 spi5.1 p2: Link is Up - 1Gbps/Full - flow control off
[ 1342.488176] sja1105 spi5.1 p1: Link is Down
[ 1444.408700] sja1105 spi5.1 trx6: Link is Up - 100Mbps/Full - flow control off
[ 1471.624407] sja1105 spi5.1 trx6: Link is Down
[ 1472.664709] sja1105 spi5.1 trx6: Link is Up - 100Mbps/Full - flow control off

root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Open Circuit
root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code OK
6.6.32-rt32-00903-g49d9f8bb25e0

1.Please compare the SJA1110 log information, check your firmware have installed successfully.

2.I tested the trx6 result of Pair A code OK, it only inserts into my converter device.

3.You also can try to test other port, such as the port as the trx5.

Hope this can help you.

BR

Joey

 

0 Kudos
Reply

5,716 Views
liujialu_2024
Contributor III

1.Please compare the SJA1110 log information, check your firmware have installed successfully.

[ 0.549758] gpio-24 (sja1110-rst-phy-t1): hogged as output/low
[ 0.555190] gpio-81 (sja1110-rst-core): hogged as output/low
[ 0.765003] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 4.447316] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 4.493501] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 4.493844] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 6.500528] sja1110: loading out-of-tree module taints kernel.
[ 6.506704] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[ 6.506721] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[ 8.091140] sja1105 spi5.1: Probed switch chip: SJA1110A
[ 9.035134] sja1105 spi5.1 p1 (uninitialized): PHY [spi5.1-base-tx:01] driver [NXP CBTX (SJA1110)] (irq=POLL)
[ 9.058996] sja1105 spi5.1: configuring for fixed/2500base-x link mode
[ 9.062630] sja1105 spi5.1: Link is Up - 2.5Gbps/Full - flow control off
[ 9.074566] sja1105 spi5.1 trx5 (uninitialized): PHY [spi5.1-base-t1:01] driver [NXP C45 TJA1103] (irq=POLL)
[ 9.088758] sja1105 spi5.1 trx6 (uninitialized): PHY [spi5.1-base-t1:02] driver [NXP C45 TJA1103] (irq=POLL)
[ 9.128177] sja1105 spi5.1 trx7 (uninitialized): PHY [spi5.1-base-t1:03] driver [NXP C45 TJA1103] (irq=POLL)
[ 9.165856] sja1105 spi5.1 trx8 (uninitialized): PHY [spi5.1-base-t1:04] driver [NXP C45 TJA1103] (irq=POLL)
[ 9.336509] sja1105 spi5.1 trx9 (uninitialized): PHY [spi5.1-base-t1:05] driver [NXP C45 TJA1103] (irq=POLL)
[ 9.372362] sja1105 spi5.1 trx10 (uninitialized): PHY [spi5.1-base-t1:06] driver [NXP C45 TJA1103] (irq=POLL)

2.I tested the trx6 result of Pair A code OK, it only inserts into my converter device.

Bold words in red is result of the command: ethtool --cable-test trx6

comandtrx6converter slaveconverter master
default slaveslavePair A code OKPair A code Unknown
ethtool -s trx6 master-slave forced-mastermasterPair A code OKPair A code OK

 

so if trx6 in slave and converter in master, it report Pair A code Unknown, 

this just be the default application of trx6.

but if trx6 in master mode, it works well always, regardless of whether the converter operates in master mode or slave mode

This is really a bit strange.

3.You also can try to test other port, such as the port as the trx5.

trx5 and trx6 are identical

0 Kudos
Reply

5,712 Views
Joey_z
NXP Employee
NXP Employee

hi,liujialu_2024

Thank you for your reply and information.

so if trx6 in slave and converter in master, it report Pair A code Unknown.

>>>How do you do your testing of Slave/master?

BR

Joey

0 Kudos
Reply

5,644 Views
liujialu_2024
Contributor III
# set trx6 in rdb2 shell
$ ethtool -s trx6 master-slave forced-slave
$ ethtool --cable-test trx6

t1-converter can swith master/slave using the dial switch
0 Kudos
Reply

5,821 Views
liujialu_2024
Contributor III

bsp 42.0

Linux s32g274ardb2 5.15.158-rt76 #1 SMP PREEMPT Wed Sep 11 13:48:24 UTC 2024 aarch64 aarch64
aarch64 GNU/Linux

0 Kudos
Reply

5,812 Views
Joey_z
NXP Employee
NXP Employee

hi,liujialu_2024

Thank you for your information and question.

Could you share more information with me?

1.Do you test the BSP42 package that have not modified?

2.How do you change the 100Base-T1 port to eth port signals for the ping testing, which device are you using?

BR

Joey

0 Kudos
Reply

5,797 Views
liujialu_2024
Contributor III

my T1-to-RJ45 device:

t1_box.jpg

Tags (1)
0 Kudos
Reply

5,802 Views
liujialu_2024
Contributor III

1.Do you test the BSP42 package that have not modified?

with bsp 42.0 default image, it report error also.

root@s32g274ardb2:~# uname -r
6.6.32-rt32-00903-g49d9f8bb25e0
root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Unknown

root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Open Circuit


root@s32g274ardb2:~# ethtool --cable-test trx6
Cable test started for device trx6.
Cable test completed for device trx6.
Pair A code Short within Pair

 

testings of Open and Short still work well.

 

 

0 Kudos
Reply

5,809 Views
liujialu_2024
Contributor III

1.Do you test the BSP42 package that have not modified?

v6.6.32 kernel does not support IPCF, so, we need v5.15.158 kernel. 

2.How do you change the 100Base-T1 port to eth port signals for the ping testing, which device are you using?

according to the S32G2_LinuxBSP_42.0_User_Manual.pdf

chapter: 7.7.3 Enabling SJA1110 DSA driver, to enable DSA of SJA1110, then

$ ifconfig trx6 down

$ ifconfig trx6 192.168.2.123 up

my PC's ip address is 192.168.2.211, so ping can work now.

 

0 Kudos
Reply