eMCEM Signal List - S32G3 SAF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMCEM Signal List - S32G3 SAF

1,526 次查看
SHIVRAJ
Contributor II

Dear Team,

I am currently working on the S32G3 Safety Framework and would like to understand more about some of the eMCEM signals — specifically:

  • A clear description of each signal
  • The need for performing the test related to it in SAF
  • The conditions or basis on which it is triggered
  • The criteria or rationale for determining how each signal should be handled
  • Any reference documents or manuals that can help understand them better

I have attached a query sheet with the details of the signals for your reference. Kindly help clarify these points at your convenience.

Looking forward to your guidance.

Best Regards,
Shivraj Chirmure

标记 (3)
0 项奖励
回复
3 回复数

1,494 次查看
Joey_z
NXP Employee
NXP Employee

hi,SHIVRAJ

Thank you for your information.

The document of S32G_SAF_EMCEM_UM.pdf(SW32G_SAF_2.0.2_QLP01_D2410/eclipse/plugins/eMcem_TS_T40D11M20I2R0/doc/S32G_SAF_EMCEM_UM.pdf), you can refer to check more information about the EMCEM.

 The corresponding explanations for the signals have been made in the Table 57.S32G2XX Fault List. Also, you can refer to RMS32G3.pdf-Chapter 68 to view the Single fault signal flow.

Hope it can help you.

BR

Joey

0 项奖励
回复

1,464 次查看
SHIVRAJ
Contributor II

Hi Joey,

Thank you for the quick response. But I'd like to understand more on how these falls are triggered.

Can you help me understand on it or give any reference to where I can read about them.

Thanks in advance!

Shivraj

标记 (3)
0 项奖励
回复

1,428 次查看
Joey_z
NXP Employee
NXP Employee

hi,SHIVRAJ

Thank you for your information.

The Error signal need to set Set corresponding error flag in NCF_Sn, and set th e NCF_En and NCF_TOEn , so the Fault state and Alarm state can be Trigger.It is as shown the following picture.

Joey_z_0-1752060706874.png

 

In addition, you can find more  information from the attachment of RMS32G3.pdf for it.

Joey_z_1-1752060830799.png

Joey_z_2-1752060838594.png

 

Hope it can help you.

BR

Joey

 

 

 

0 项奖励
回复