bitbake gcc giving do_compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake gcc giving do_compile error

Jump to solution
1,149 Views
hulk101
Contributor III

Hi,
I have encountered a gcc do_compile issue with ubuntu 24.04.
Machine - S32G2-VNP-GLDBOX
Userguide - https://github.com/nxp-auto-linux/auto_yocto_bsp/tree/release/bsp38.0?tab=readme-ov-file

Error log:
ERROR: gcc-cross-aarch64-11.3.0-r0 do_compile: oe_runmake failed
ERROR: gcc-cross-aarch64-11.3.0-r0 do_compile: ExecutionError('/mnt/3231a06d-ea48-8393-9819fa8g54d6/S32G2/xen_build/BSP38/build_s32g274ardb2/tmp/work/x86_64-linux/gcc-cross-aarch64/11.3.0-r0/temp/run.do_compile.3892204', 1 , None, None)

S32G-VNP-RDB2 

Labels (1)
0 Kudos
Reply
1 Solution
1,131 Views
Joey_z
NXP Employee
NXP Employee

hi,NXPUser1234

Thank you for your question.

You can refer to the S32G2_LinuxBSP_38.0_User_Manual.pdf, and check the package and environment for your using.

Joey_z_0-1751598532737.png

Hope it can help you.

BR

Joey

 

View solution in original post

0 Kudos
Reply
1 Reply
1,132 Views
Joey_z
NXP Employee
NXP Employee

hi,NXPUser1234

Thank you for your question.

You can refer to the S32G2_LinuxBSP_38.0_User_Manual.pdf, and check the package and environment for your using.

Joey_z_0-1751598532737.png

Hope it can help you.

BR

Joey

 

0 Kudos
Reply