Yacto project for S32G3 GoldVIP error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yacto project for S32G3 GoldVIP error

775件の閲覧回数
Wzlinux
Contributor III

Hi deai NXP

I follow UM12007 do the yaoto project for goldvip. 

in the 25.2.2 there is a  source nxp-setup-alb.sh -D fsl-goldvip \
-m s32g399ardb3goldvip \
-e "meta-aws meta-java" command.

there is a error after this command . Please help to take a look at this issue. thank you.

Wzlinux_0-1739505383849.png

Wzlinux_1-1739505428055.png

Wzlinux_2-1739505437000.png

 

 

 

タグ(1)
0 件の賞賛
返信
1 返信

737件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Wzlinux 

Thanks for your post.

May I know which version Goldvip you were working with?

I have tested with 1.12, and seems there are no issue.

"source nxp-setup-alb.sh -D fsl-goldvip-hv \-m s32g399ardb3goldvip \-e "meta-aws meta-java"
Configuring for s32g399ardb3goldvip and distro fsl-goldvip-hv...

Proprietary and third party software is subject to agreement and compliance
with, NXP's End User License Agreement. To have the right to use these
binaries in your images, you must read and accept the following terms. If
there are conflicting terms embedded in the software, the terms embedded in
the Software will control.

.................."

I  suggest trying it the following way:

 

BR

Chenyin

0 件の賞賛
返信