Using the "EB" tool to refer to "AN13750" for configuration errors in "Bootloader_S32G2XX_aSR_4.4_S7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the "EB" tool to refer to "AN13750" for configuration errors in "Bootloader_S32G2XX_aSR_4.4_S7

396件の閲覧回数
lion_6
Contributor I

When I use the "EB" tool to refer to "AN13750" to configure "Bootloader_S32G2XX_aSR_4.4_S7", the following error occurs and it prompts that there is no license. How can I solve it?At the same time, I have successfully imported 'SW32G-RTD-4.4_3.0.2.HF01. link' into EB

lion_6_0-1750848658644.png

 

0 件の賞賛
返信
5 返答(返信)

316件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @lion_6 

Thanks for your reply.

From the logs shared, seems the license is not well detected by the EB, I suggest reinstalling both EB and corresponding license administrator(removing all EB related packages first, and then reinstall 27.1 and corresponding license administrator software), furthermore, would you mind also sharing the downloading page for EB in your account? (just mask the license number)

 

BR

Chenyin

0 件の賞賛
返信

344件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @lion_6 

Thanks for your confirmation.

According to the AN13750, 

chenyin_h_0-1750919463886.png

I suggest using the EB27.1 for another trial, from my experience, most S32G software packages are developed and tested with EB27.1 version.

 

BR

Chenyin

0 件の賞賛
返信

332件の閲覧回数
lion_6
Contributor I

Hello @chenyin_h ,
I tried downloading version 27.1.0, but still have the same problem. It seems to be a license issue and some modules are missing. Is there any other solution?
Thank you!

lion_6_0-1750924482813.png

 

0 件の賞賛
返信

367件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @lion_6 

Thanks for your post.

May I know which version bootloader you are working with? also, may I know the EB version used in your work? Is it downloaded from your NXP account and had activated by the license shown in your download page?

 

BR

Chenyin

0 件の賞賛
返信

359件の閲覧回数
lion_6
Contributor I

Hello, @chenyin_h 

Thanks for the reply.

My EB version is 29.2.0
The activation status is shown in the following figure:

lion_6_0-1750906962987.png
In terms of software, I followed the instructions mentioned in the "AN13750" manual:
SDK version: Integration-Reference_Samples_32G2_2022_06
RTD version: SW32G_STD-4.4_3.0.2HF01




0 件の賞賛
返信