[Urgent] Question about SRAM ECC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Urgent] Question about SRAM ECC

Jump to solution
2,981 Views
harry_choi
Contributor IV

Dear Community,

I have several questions about SRAM ECC.

1) Is the ECC on SRAM enabled by default? Which codes make the ECC on SRAM enabled?

2) I'm trying to launch A53 core from M7 core, so I have to copy u-boot code to SRAM. But I knew that I have to enable __RAM_INIT flag in linker to init ECC. If not, the exception happened when I copy the u-boot code to SRAM. Is that normal symptom?

3) Initializing SRAM area(uboot code to be copied) during booting time takes so long time. Is there any fast way to reduce SRAM initialization time? or is there any way to disable ECC on special area of SRAM?

Best Regards,

Harry

0 Kudos
Reply
1 Solution
2,962 Views
harry_choi
Contributor IV

I found the solution by myself.

Thanks!

View solution in original post

0 Kudos
Reply
2 Replies
2,963 Views
harry_choi
Contributor IV

I found the solution by myself.

Thanks!

0 Kudos
Reply
2,550 Views
SherlockInSpace
Contributor I
Hey Harry, can you share what you found as answers to your questions?
0 Kudos
Reply