[Urgent] Question about SRAM ECC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Urgent] Question about SRAM ECC

ソリューションへジャンプ
2,998件の閲覧回数
harry_choi
Contributor IV

Dear Community,

I have several questions about SRAM ECC.

1) Is the ECC on SRAM enabled by default? Which codes make the ECC on SRAM enabled?

2) I'm trying to launch A53 core from M7 core, so I have to copy u-boot code to SRAM. But I knew that I have to enable __RAM_INIT flag in linker to init ECC. If not, the exception happened when I copy the u-boot code to SRAM. Is that normal symptom?

3) Initializing SRAM area(uboot code to be copied) during booting time takes so long time. Is there any fast way to reduce SRAM initialization time? or is there any way to disable ECC on special area of SRAM?

Best Regards,

Harry

0 件の賞賛
返信
1 解決策
2,979件の閲覧回数
harry_choi
Contributor IV

I found the solution by myself.

Thanks!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,980件の閲覧回数
harry_choi
Contributor IV

I found the solution by myself.

Thanks!

0 件の賞賛
返信
2,567件の閲覧回数
SherlockInSpace
Contributor I
Hey Harry, can you share what you found as answers to your questions?
0 件の賞賛
返信