Uboot Read SRAM failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot Read SRAM failed

1,364 Views
Coco111
Contributor III

I am debugging S32G3 IPCF and

I found that in the u-boot terminal, I cannot use md 0x34000000 to obtain the content of sram

(note:S32G2 is ok)

Screenshot from 2023-07-12 14-42-19.pngScreenshot from 2023-07-12 14-42-19.png

Tags (3)
0 Kudos
Reply
1 Reply

1,350 Views
nxf92355
NXP Employee
NXP Employee

Hi Ni Yu

 

Hope you are doing well

There my be problem with cache, try below command in u-boot

=> dcache off

=> md.b 0x34000000 0x10

the result with my board as below

Screenshot from 2023-07-13 11-26-56.pngScreenshot from 2023-07-13 11-26-56.png

 

Regards ,

Tushar

0 Kudos
Reply