UART_1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART_1

3,481件の閲覧回数
vimalrajendran
Contributor II

Hi ,

      i am using s32G2 board i using uart1 pin PA_13 for TX and PB_10 for RX. but i cant read GPS data. can you give me some suggestion.

This two pin possible for UART or NOT?

 

Thanks

Vimal

 

 

0 件の賞賛
返信
3 返答(返信)

3,454件の閲覧回数
vimalrajendran
Contributor II

Hi Bulat,

              in s32g2gen2.dtsi file or linflexuart.c driver file are you telling?

0 件の賞賛
返信

3,468件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, PA_13 can be used UART1 TX and PB_10 as UART1 RX. Please check if pins are correctly configured and LINFlexD_1 is set to UART mode in your case.

Use a scope to check pins for UART activity.

 

Regards,

Bulat

 

0 件の賞賛
返信

3,033件の閲覧回数
niranjpo
Contributor I

Hi Bulat,

How UART activity will be generated from u-boot to probe pins on scope. 

There is no uart related function in u-boot.

 

Regards,

Niranjan

0 件の賞賛
返信