To check LPDDR4 for S32G2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

To check LPDDR4 for S32G2

跳至解决方案
5,190 次查看
Henry_Mei
Contributor III

Hi,

Have a good day.

Can you check if below Micron part is compatible for S32G?

MT53E1G32D2FW-046AUT:A

Br,

Henry

标记 (1)
0 项奖励
回复
1 解答
5,160 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, is also compatible with S32G2.

Regards

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,617 次查看
swhite39
Contributor II

Hi there,

Would you be able to check if the "MT53D1024M32D4DT-046 AUT:D" is compatible with the S32G2?

I am having some issues using the DDR Tool, and I wasn't sure if the issues could be related to the DDR chip selection.

Thanks,
Scott


0 项奖励
回复
4,186 次查看
SureshBabuV531
Contributor I

How to configure LPDDR4 in s32g274? Do we have any driver available to do read and write operations?

0 项奖励
回复
5,186 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Henry_Mei,

The 17 ROW addressing LPDDR4 has been veried on S32G3 EVB. the DRAM partnumber is MT53E1G32D2FW-046 AUT:A

LPDDR4 DRAM configurations supported in S32G3, But please note that the maximum density supported in S32G3 is 4GB only. S32G3 memory map does not allow to go beyond 4GB DRAM space.

So, if customer has LPDDR4 DRAM of 16Gb density per channel per die (with ROW17 support), then single rank dual channel dual die can configure in S32G3 ddr controller because the total density will be 32Gb/4GB for two channels.

Similarly, if customer has LPDDR4 DRAM of 8Gb density per channel per die, then dual rank dual channel DRAM can be configured with S32G3 to make 32Gb/4GB as total density (this configuration of DRAM does not require ROW17 support).

Regards

0 项奖励
回复
5,165 次查看
Henry_Mei
Contributor III

Hi,

Thanks for your reply.

I understood, the part number is ok for S32G3, but the application focuses on S32G2.

Is Micron part  compatible for S32G2?  It is verified on S32G2?

MT53E1G32D2FW-046AUT:A

Many thanks.

Henry

0 项奖励
回复
5,161 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, is also compatible with S32G2.

Regards

0 项奖励
回复
5,135 次查看
Henry_Mei
Contributor III

Hi,

Have a good day.

Thank you for your strong support.

Br,

Henry

0 项奖励
回复