The VLAN ID is incorrect when multicast data is sent

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The VLAN ID is incorrect when multicast data is sent

2,518件の閲覧回数
B0
Contributor I

The PFE driver version we used is as follows:
PFE-DRV_S32G_A53_QNX_RTM_1.0.0

In QNX 7.0 system, we configure VLAN 10 based on PFE0. The VLAN configuration method is as follows:
ifconfig vlan10 create
ifconfig vlan10 vlan 10 vlanif pfe0
ifconfig vlan10 172.16.110.11 netmask 255.255.255.0 up
However, when sending data through multicast(from 172.16.110.11  to 239.5.x.x), I capture packets through tcpdump and find that the VID is 7. How can I solve this?

ラベル(1)
0 件の賞賛
返信
1 返信

2,500件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello B0,

 

This issue is from QNX i guess someone will help you, or better move to QNX forum.

 

Regards

0 件の賞賛
返信